Windows alone is not enough
Applications that need sub-millisecond response times, predictable execution of control processes, require extremely accurate time control based on a constant time sampling. Windows is not deterministic and has not been designed to fulfill the needs of real-time control.
Then to impose accurate, time critical processing requirements, a hard real-time operating system is required in order to enable Windows environment to control tasks. INtime is the only RTOS designed to run side-by-side to Windows.
The real-time kernel being part of KAS contains inter-process communication and synchronization mechanisms to guarantee a real-time control of your automation system.
Real-time computations can be said to have failed if they are not completed before their deadline, where their deadline is relative to an event. A real-time deadline must be met, regardless of system load.
For the KAS Simulator, KAS relies on Windows capabilities.
|
Copyright © 2015 Kollmorgen™ |
|